DIO#.SOURCE
Description
Gets or sets the bi-directional output source for channel x when configured as a digital output (see DIO#.DIR).
| Value | Description |
|---|---|
| 0 - User | User controls the output value using DIO#.STATEU |
| 1 - Action Table | Action table controls the output value |
Examples
Usage
When DIO#.SOURCE = 0 (User) and DIO#.DIR = 1 (output), then DIO#.STATE will be controlled by DIO#.STATEU.
When DIO#.SOURCE = 1 (Action table) and DIO#.DIR = 1 (output), then DIO#.STATE will be controlled by the assigned action, if any.
If DIO#.DIR = 0 (input) then the DIO#.SOURCE parameter is ignored.
Code
Changing output state with STATEU and then changing SOURCE to be action table with no action configured:
--> DIO1.DIR 1 (output) --> DIO1.SOURCE 0 (user) --> DIO1.STATE 0 --> DIO1.STATEU 1 --> DIO1.STATE 1 --> DIO1.SOURCE 1 //Action table --> DIO1.STATE 0
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
DIO1.SOURCE | 0x368A | 0x5 | USINT | - | - | RW | False |
| DIO2.SOURCE | 0x368B | 0x5 | USINT | - | - | RW | False | |
| DIO3.SOURCE | 0x368C | 0x5 | USINT | - | - | RW | False | |
| DIO4.SOURCE | 0x368D | 0x5 | USINT | - | - | RW | False | |
| DIO5.SOURCE | 0x368E | 0x5 | USINT | - | - | RW | False | |
| DIO6.SOURCE | 0x368F | 0x5 | USINT | - | - | RW | False |